Start
> notebooks/laptops
> Acer LX.AZK0J.001
|
 |
Aspire 3682WXMi |
|
Brand: Acer
Product code: LX.AZK0J.001
EAN/UPC code: 0099802859107
|
Category: notebooks/laptops
|
|
|
|
|
Release date: 15 Dec 2006
Info modified on: 07 2008 09:19:57
legitieme Windows® XP Media Center Edition 2005, Intel® Celeron® M Processor 420 (1.6GHz/1MB/533MHz), 14.1TFT WXGA, 1024MB DDR RAM (2x 512), 80GB HDD, DVD-RW Dual Double Layer, 6-cell LiIon, 56K modem, Wired & Wireless Lan 802.11g, Intel® GMA950 128MB shared, no S-video, no IEEE-1394, no FIR, 0.3MP Orbicam, 5-in-1 card reader
|
|
|
|
|
|
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
|
 |
 |
 |
|
|
The Aspire 3680 is designed to provide a complete home and business solution offering performance, flexibility, empowerment and value in a compact notebook. Featuring an Intel® Celeron® processor, full wired and wireless connectivity and a stunning 14.1” WXGA CrystalBrite display, with optional, integrated 0.3MP videocamera, the Aspire 3680 brings productivity and entertainment to a new level.
|
|
 |
Specs
|
Alternatives
|
Options
|
|
|
|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1600 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Celeron Mobile
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Intel Celeron M 420
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
533 MHz
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
1 MB
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
80 GB
|
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
14.1 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
WXGA TFT LCD
|
|
Display resolution
|
|
Resolution of the display for the system
1280 x 800 pixels
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
1024 MB
|
| Internal memory type |
DDR II RAM |
| Compatible memory cards |
SD/MMC/MS/MS Pro/xD |
| Graphic adapter |
Intel GMA 950 |
|
Maximum graphic adapter memory
|
|
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
128 MB
|
|
Optical drive type
|
|
Type of the optical drive
DVD±RW DL
|
| Audio system |
Intel High Definition Audio |
| Number of built-in speakers |
2 |
| Camera included |
 |
|
Megapixel
|
|
MegaPixels: The number (in millions) of light-sensitive picture elements, or pixels, actually used by the camera's image sensor (CCD) to record light, and which are reflected to the final number of recorded pixels stored on the memory card.
0.3 MP
|
| Internal modem |
 |
| Networking features |
Ethernet/Fast Ethernet |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11b/g |
| Modem speed |
56 Kbit/s |
| Modem type |
ITU V.92 |
| Wake-on-LAN ready |
 |
| Wireless LAN data transfer rate (max) |
54 Mbit/s |
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|
|
|
|
|
|
|
| | |