|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1700 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Pentium Mobile
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Pentium M 735
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
400 MHz
|
|
Chipset
|
|
Chipset for this configuration; expressed as manufacturer and coined name
Intel 915GM Express
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
2 MB
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
80 GB
|
| Hard disk interface |
Ultra-ATA/100 |
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
4200 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
15 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
TFT LCD
|
|
Number of colours
|
|
Maximum number of viewable colors.
16.7 M
|
|
Display resolution
|
|
Resolution of the display for the system
1024 x 768 pixels
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
512 MB
|
|
Memory slots
|
|
Number and type of memory expansion slots; including connector and memory module descriptions
2
|
| Internal memory type |
DDR2 |
| Maximum internal memory |
2 GB |
| Graphic adapter |
Intel GMA 900 |
|
Maximum graphic adapter memory
|
|
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
128 MB
|
|
Optical drive type
|
|
Type of the optical drive
DVD-Dual DL
|
| Built-in microphone |
 |
| Number of built-in speakers |
2 |
| Keyboard layout |
QWERTY |
| Hot keys |
4 |
| Number of keyboard cursor keys |
4 |
| Keyboard function keys |
12 |
| Windows keys |
 |
| Camera included |
 |
| Internal modem |
 |
| Networking features |
Fast Ethernet, WLAN |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11b/g |
| Modem speed |
56 Kbit/s |
| Modem type |
ITU V.92 |
| Wake-on-LAN ready |
 |
|
Cabling technology
|
|
Type of cable technology performance; including the fiber or cable type
10/100Base-T(X)
|
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|