Start
> notebooks/laptops
> Acer LX.TL70X.038
|
 |
TravelMate 7520-401G16Mi |
|
Brand: Acer
Product code: LX.TL70X.038
EAN/UPC code: 0099802085728
|
Category: notebooks/laptops
|
|
|
|
|
Release date: 02 Sep 2007
Info modified on: 21 Aug 2008 21:21:39
Legitimate Windows Vista® Home Premium, AMD Mobile Turion™ 64 X2 Dual-Core processor TL58 (1.9GHz), Microsoft® Office Ready 2007 (trial version), 17TFT WXGA+ CrystalBrite, 1024MB DDR II RAM (2x 512), 160GB HDD (5400rpm), Super Multi DVD-RW Double Layer, 6-cell LiIon, 56K modem, Gigabit & Wireless Lan 802.11b/g, ATI Radeon™ Xpress 1250 up to 384MB HyperMemory shared, 5-in-1 card reader, 0.3MP CrystalEye
|
|
|
|
|
|
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
|
 |
 |
 |
|
|
The Acer TravelMate 7520 has everything companies need to maximize their business performance. Boasting a superb 17” widescreen TFT panel and equipped with the powerful AMD Turion™ 64 X2 Mobile Technology it provides a complete solution for today’s demanding business users at great value. The 17” wide TFT panel with optional integrated Acer CrystalEye webcam, up to two large serial-ATA hard
...
More>>>
disc drives, the latest wireless technology and Acer’s innovative Empowering Technology (a complete suite of productivity-enhancing tools) make the new TravelMate 7520 the perfect example of Acer’s strategy to provide powerful tools to business customers that want to take business productivity to the next level.
Business optimized Acer has equipped the TravelMate 7520 with the Acer CrystalEye webcam, allowing real-time face-to-face video conferencing for a maximum on productivity and flexibility, mounted at the top of a brilliant 17” LCD panel. For additional expandability of the storage capacity, the TravelMate 7520 can also be equipped with a 2nd hard disk drive for an optimal enlargement. Connectivity The TravelMate 7520 is a complete communication instrument that allows professional users to seamlessly switch from different connectivity options: using the latest N wireless card enhanced by Acer SignalUp™ with InviLink™ Nplify™ wireless technology, to offer the fastest wireless speeds available today or optional an 802.11 b/g wireless solution, WPAN connection with optional built-in Bluetooth 2.0 module and wired LAN connection with the Gigabit Ethernet card and the integrated modem.
<<<Less
|
|
 |
Specs
|
Alternatives
|
Options
|
|
|
|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1900 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
AMD Turion 64 X2 Mobile
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
AMD Turion 64 X2 TL-58
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
160 GB
|
| Hard disk interface |
SATA |
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
17 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
WXGA+ TFT LCD
|
|
Display resolution
|
|
Resolution of the display for the system
1440 x 900 pixels
|
|
Number of colours
|
|
Maximum number of viewable colors.
16.7 M
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
1024 MB
|
|
Memory slots
|
|
Number and type of memory expansion slots; including connector and memory module descriptions
so-DIMM
|
| Internal memory type |
DDR2 SDRAM |
|
Memory layout
|
|
Describe how memory is plugged on the motherboard
2 x 512 MB
|
| Maximum internal memory |
4 GB |
| Compatible memory cards |
SD/MMC/MS/MS Pro/xD |
| Graphic adapter |
ATI Radeon Xpress 1250 |
|
Maximum graphic adapter memory
|
|
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
384 MB
|
|
Optical drive type
|
|
Type of the optical drive
DVD±RW DL
|
| Audio system |
MS-Sound |
| Number of built-in speakers |
2 |
| Keyboard function keys |
12 |
| Keyboard number of keys |
105 / 106 |
| Camera included |
 |
|
Megapixel
|
|
MegaPixels: The number (in millions) of light-sensitive picture elements, or pixels, actually used by the camera's image sensor (CCD) to record light, and which are reflected to the final number of recorded pixels stored on the memory card.
0.3 MP
|
| Internal modem |
 |
| Networking features |
Gigabit Ethernet |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11b/g |
| Modem speed |
56 Kbit/s |
| Modem type |
ITU V.92 |
| Wake-on-LAN ready |
 |
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|
| Wireless LAN data transfer rate (max) |
54 Mbit/s |
| Operating system provided |
Windows Vista Home Premium Edition |
|
| Bundled software |
Acer Empowering Technology (eNet, ePower, ePresentation, eDataSecurity, eLock, eRecovery, eSettings Management), Acer GridVista™, Acer Launch Manager, Adobe® Reader®, CyberLink® PowerDVD™, NTI CD Maker™, NTI Shadow™ |
| Battery technology |
Lithium-Ion |
|
Battery life
|
|
Maximum battery life in hours. Mobile Mark™ (2002) is the standard often used to benchmark battery life time. In some cases battery life can be extended by adding extra batteries.
2.5 h
|
| Number of battery cells |
6 pcs |
| ExpressCard slot |
 |
| VGA (D-Sub) ports quantity |
1 |
| Ethernet LAN (RJ-45) ports quantity |
1 |
|
TV out port
|
|
Description of TV Out port
|
|
USB 2.0 ports quantity
|
|
USB 2.0 ports have a data transmission speed of 480 Mbps, and are backwards compatible with USB 1.1 ports. You can connect all kinds of peripheral devices to them.
4
|
| Modem (RJ-11) ports |
1 |
| Speaker/ headphone/ line-out jack |
 |
| Microphone, line-in jack |
 |
| S/PDIF out port |
 |
| DC-in jack |
 |
| DVI port |
 |
|
Infrared data port
|
|
A data port that uses infra-red data association (irDA) as the standard for wireless communications between computer and mobile phone devices. For example, to update the phone list on your irDA-enabled PC, you would line up the infra-red ports on each device and then transfer the phone information to your PC. This is a wireless transfer, so you don't need a cable or extra software.
|
| CardBus PCMCIA slots quantity |
1 |
| SmartCard slot |
 |
| CardBus PCMCIA slot type |
Type II |
| TV in port |
 |
| Port replicator |
 |
| Cable lock slot |
Kensington |
| BIOS password |
 |
|
Weight
|
|
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
3660 g
|
|
Dimensions W x D x H
|
|
Dimensions of the produkt (Width x Depth x Height) in millimeter.
400 x 290 x 43 mm
|
| Depth |
290 mm |
|
Height
|
|
Height of the product
43 mm
|
| Width |
400 mm |
| Type |
PC |
| Pointing device |
Touchpad |
|
|
|
|
|
| computers |
 |
 |
PX1441E-1NSK |
17" Notebook Starter Kit V - Entry level case, Mouse, USB Hub |
|
| components |
 |
|
NS-LC100 |
NOTEBOOK KOELER NEWSTAR LC-100 |
|
| hard disk drives |
 |
 |
Case-USB218-40BL |
HT-18A |
|
 |
 |
Case-USB218-60 |
HT-18A |
|
 |
 |
CASE-USB218-20BL |
HT-18A |
|
 |
 |
SPE3030CC/00 |
External Hard Disk, 320GB |
|
| Show all hard disk drives >> | | keyboards & desktops |
 |
 |
313518 |
Wireless Keyboard & Mouse Belinea o.board US White |
|
 |
 |
KP002 |
Portable USB Keypad and 2 Port HUB |
|
| flash memory |
 |
 |
SI-707134 |
Flash Drive With Encryption Software 8GB |
|
| network cards & adapters |
 |
 |
DWA-140 |
Wireless N USB Adapter |
|
 |
 |
20002325 |
FRITZ!WLAN USB Stick |
|
 |
 |
20002420 |
FRITZ!WLAN USB Stick N |
|
 |
 |
3CRUSB10075 |
OfficeConnect Wireless 54Mbps 11g Compact USB Adapter |
|
 |
 |
CN-WF518D |
Network Adapter, Wireless, 54Mbps, Retail, IEEE 802.11b/IEEE 802.11g, USB 2.0 |
|
 |
 |
Z 14438 Z |
Link Z 14438 Z |
|
 |
 |
DWA-645 |
RangeBooster N650 Draft-11n PC Card |
|
| Show all network cards & adapters >> | | notebook bags & cases |
 |
 |
CNXL1 |
XL Computer Case |
|
 |
 |
CN317 |
XL Notebook Case |
|
 |
 |
TCG200 |
City.Gear XL Messenger Notebook Case |
|
 |
 |
PX1418E-1NCA |
More4You Carry Case Value Edition 17" |
|
 |
 |
VNC17 |
Basic nylon laptop case 17" |
|
 |
 |
N 7828 A |
AluCompact |
|
| Show all notebook bags & cases >> | | mice |
 |
 |
CLLMTRAVEL |
Lounge’n’LOOK Travel Mouse |
|
 |
 |
MI015 |
Mini Wireless Optical Mouse |
|
 |
 |
MICROII-EU |
USB optical micro mouse |
|
 |
 |
931669-0914 |
V450 Laser Cordless Mouse for Notebooks |
|
 |
 |
AI-707911 |
Wireless Optical Notebook Mouse |
|
| Show all mice >> | | antivirus & security software |
 |
 |
2869 |
AntiVirus 2008 NL |
|
 |
 |
2867 |
TotalCare 2008 NL |
|
 |
 |
2870 |
InternetSecurity 2008 NL |
|
 |
 |
Q12P08 |
Internet Security 2008, 3-user, 1 Year, NL |
|
 |
 |
KL1125NLBOX |
Kaspersky® Anti-Virus 7.0, CROM, Box, NL |
|
| | | | |