|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
2400 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Core 2 Duo
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Intel Core 2 Duo T8300
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
800 MHz
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
3 MB
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
500 GB
|
| Hard disk interface |
SATA |
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
20.1 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
WSXGA+ TFT LCD
|
|
Display resolution
|
|
Resolution of the display for the system
1680 x 1050 pixels
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
4096 MB
|
| Internal memory type |
DDR2 SDRAM |
|
Memory layout
|
|
Describe how memory is plugged on the motherboard
2 x 2048 MB
|
| Maximum internal memory |
4 GB |
| Compatible memory cards |
SD/MMC/MS/MS Pro/xD |
| Graphic adapter |
NVIDIA GeForce 8800M GTS |
|
Maximum graphic adapter memory
|
|
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
1791 MB
|
|
Optical drive type
|
|
Type of the optical drive
Blu-Ray DVD±RW
|
| Built-in microphone |
 |
| Audio system |
3D Sound Blaster Pro |
| Built-in subwoofer |
 |
| Number of built-in speakers |
2 |
| TV tuner type |
DVB-T |
| Camera included |
 |
| Internal modem |
 |
| Networking features |
Gigabit Ethernet |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11a/g/n |
| Modem speed |
36 Kbit/s |
| Bluetooth version |
2.0+EDR |
| Wake-on-LAN ready |
 |
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|
| Operating system provided |
Windows Vista Home Premium Edition |