A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
Specs
Alternatives
Options
Disk drive
Hard disk drive capacity
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
160 GB
Disk drive
Hard disk rotational speed
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
Memory
Internal memory
The amount of memory measured in megabytes installed in the system's hardware