Start
> netbooks
> MSI U100W-005NL
|
 |
Wind U100W-005NL White |
|
Brand: MSI
Product code: U100W-005NL
EAN/UPC code:
|
Category: netbooks
|
|
|
|
|
Release date: 23 May 2008
Info modified on: 09 2008 16:48:17
Wind U100W-005NL - Intel Atom N270 1.6GHz, 1024MB, 80GB, 10” 1024x600 LCD, WLAN, Bluetooth, Webcam, WinXP HE, White
|
|
|
|
|
|
| Small-sized, low-cost, light weight, lean function subnotebooks optimized for Internet access and core computing functions (e.g., word processing) — either directly from applications installed on the netbook itself or indirectly, via cloud computing. |
 |
 |
 |
|
|
Ride with the Wind
The Freedom to Watch 10” Wide LCD Display The U100 has selected a 10” wide LCD display as oppose to the typical smaller sizes to provide better comfort while viewing or reading. In addition, the 1024x 600 resolution can relief concerns of the full display of WebPages while browsing, giving you the freedom when exploring the internet. The
...
More>>>
Latest in LED Power-Saving Backlight Technology The U100 is embedded with the LED power-saving backlight technology in providing better color fullness and brightness, elevating the total quality of imagery. Furthermore, the lower usage of power can offer a longer operating time. Convenient Magnifying Capability The U100 is equipped with the capability of magnifying text within software, so you may magnify any of the words displayed on the monitor freely, making it easier when you are viewing photos, editing or reading documents.
The Freely to Go Lightness in Design The frame is approximately 26 centimeters in length and 18 centimeters in width. It is only 19-31.5 mm in thickness making it extremely thin. The total weight added with the battery is not more than 1 kilogram, making the U100 very ideal for taking it on the go.
The Freely to Operate Ergonomic Big-Size Keyboard and Touch Pad MSI has the same persistence for proper ergonomically design even on the keyboards of our smaller notebook computers. The keyboard of the U100 not only has great texture, it also increased the space between the keys to 17.5mm, allowing you to be as comfortable as you can. Plus, ingeniously designed spacebar and touchpad, so your fingers can move smoothly while avoiding strain. Hard Drive with Massive Capacity Unlike its other competitors that has compromised the memory capacity to decrease in size, the U100 is equipped with the 2.5 inch standard hard drive 80G*. It can operate just as any other notebook computers; without the worries of not having enough memory capacity to record the greatest moments in life. The Newest Intel® Atom™ Processor Intel® Atom™ Processor uses a brand new design structure as basis adding in as much as 47 million transistors into one single chip, and the size is not even 25 (mm)². This is smallest and uses the least energy (power usage in limited below 1 to 2.5 watts) Intel processors thus far. Not only so, this processor has more than enough mobility and outstanding functions so our users can to have complete access to the resourceful internet. Always staying connected to the variety and options of entertainment.
The Freely to Play The Excitement of Instant Communication Equipped with high resolution webcam, high-performance 2 channel stereo speakers, and microphone, all fitted perfectly within the framework design, expressing the slickness of technology and the elegance of modern fashion. Web-chats can be broadcasted instantly not missing one exciting moment. The photos taken is very sharp in resolution and brilliant in colors, capturing precise imagery both indoor or out, adding more fun to instant messaging. Wireless Internet Connection The U100 has the 802.11b / g wireless all region internet connection and Bluetooth transmission interface, so you can enjoy the convenience of accessing the internet at home or out. There will be absolutely no obstacles getting around your daily life. Comprehensive Multi-Media Application Interface U100 offers a complete entertainment interface, which includes the 4 in 1 Card Reader (applicable to SD. MMC, MS, and MS Pro), so it may meet the standards of the mainstream memory cards, making it easy to upload digital files into the notebook computer. Our focus was on the common products in the market, such as PDA’s, digital cameras, digital video cameras, digital MP3 Players, Global GPS Systems and such, also connecting to the U100 through USB 2.0 Port. An external DVD burner may be added (optional) to play and burn important files at will. Long Lasting Battery Life The last battery life can escalate the mobility and the productiveness of the U100, which can also make your daily lives much more convenient.
<<<Less
|
|
 |
Specs
|
Alternatives
|
Options
|
|
|
|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1600 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Pentium Mobile
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Intel Atom
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
533 MHz
|
|
Chipset
|
|
Chipset for this configuration; expressed as manufacturer and coined name
Intel 965GMS+ICH7M
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
0.512 MB
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
1024 MB
|
| Internal memory type |
DDR2 |
| Maximum internal memory |
2 GB |
| Memory clock speed |
667 MHz |
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
80 GB
|
| Compatible memory cards |
SD/MMC/MS/MSpro |
| Card reader integrated |
 |
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
10 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
Wide LED
|
|
Display resolution
|
|
Resolution of the display for the system
1024 x 600 pixels
|
| Graphic adapter |
UMA |
| Number of built-in speakers |
2 |
| Camera included |
 |
|
Megapixel
|
|
MegaPixels: The number (in millions) of light-sensitive picture elements, or pixels, actually used by the camera's image sensor (CCD) to record light, and which are reflected to the final number of recorded pixels stored on the memory card.
1.3 MP
|
|
|
|
|
|
|
|
|
|
|
|
|