The mouse is the second most important way of communicating with a computer. Please be careful to choose the right type of connection when buying a mouse, there are three different types: - USB is the most modern. You can recognize it by the rectangular connector. - PS/2 connectors are round. This type of connection is fairly commonly used in PC's. - Bluetooth is another modern (wireless) connection method.
World's First Bluetooth Wireless Trackball Reliable, 2nd generation Bluetooth wireless connectivity. Long-life rechargeable battery system. Small enough that anybody can comfortably wrap their entire hand over the top. Simple. Elegant. Beautiful. The Ball is the result of a three-year research and design effort into the way people use trackballs. Our goal was to find out why such
...
More>>>
a practical input device has fewer users than should be expected. Then, we wanted to create a product that was more appealing and that could make a larger number of people happy using a trackball. We believe that we succeeded.
Not Your Father's Trackball The Ball is much smaller than other 'regular size' trackballs. While keeping an industry standard ball size, we managed to shrink the housing about 30% to 50% smaller than normal. Why?... so that you can comfortably lay your hand on the top of The Ball, and your fingers will easily curl all the way around to reach the front-mounted scroll wheel. The Ball has left and right buttons, a scroll wheel, and a scroll wheel button. It's a 'pair it and work' device for any Bluetooth enabled Mac or Win XP system.
Perhaps The Best Trackball Of All Time The Ball will appeal to anyone wanting the stability and accuracy of a trackball, and the clutter-free operation of a wireless connection. Your order will include The Ball, the USB mini charging cradle, a pair of 750mAh Nickel Metal Hydride rechargeable AAA batteries, and instructions and warranty materials.
<<<Less
Specs
Alternatives
Options
Input device
Interface
Interface ports to connect pieces of equipment. USB (Universal Serial Bus) has become the most popular wired interface to connect peripherals. USB 2.0 supports speeds up to 480 Mbit/s (USB 1: 12 Mbit/s). The wireless interface FireWire is also known as the IEEE 1394 standard. Enhanced IDE (EIDE)is sometimes referred to as Fast ATA, Fast IDE or ATA-2.
USB
Buttons quantity
1
Connectivity technology
Wireless
Movement detection technology
Trackball
Scroll wheel
Platform
Mac compatibility
System requirements
Compatible operating systems
List of desktop operating systems tested as compatible with this product, including coined name and version