|
Megapixel
|
|
MegaPixels: The number (in millions) of light-sensitive picture elements, or pixels, actually used by the camera's image sensor (CCD) to record light, and which are reflected to the final number of recorded pixels stored on the memory card.
2.2 MP
|
| Data compression |
JPEG (EXIF) |
|
Digital zoom
|
|
Indicates the digital zoom capacity, the number of times that the picture is enlarged thanks to digital technology.
2 x
|
|
Optical zoom
|
|
Indicates the optical zoom capacity, the number of times that the picture can be enlarged with the optics of the camera.
3 x
|
|
Aperture range
|
|
Aperture range of the lens of the camera, expressed in f-stops
F2.8 - F5.6
|
|
Camera CCD sensor
|
|
CCD (Charged Coupled Device): A silicone chip comprised of millions of tiny, square light-gathering diodes called Picture Elements, or pixels, laid out in a checkerboard pattern. This is the "film" of a digital camera. The light data gathered from these tiny pixels needs to be "processed" by the camera's image processor into Recorded Pixels.
Super CCD: A proprietary CCD system, produced by Fujifilm, that utilizes larger, octagonal-shaped, light-gathering diodes called Picture Elements, or pixels, that are laid out in a saw-tooth pattern. Super CCDs can capture more light information than ordinary CCDs; the extra information is used by the camera's image processor to improve color accuracy and ISO Speed.
Super CCD HR (High Resolution): Is capable of nearly doubling the Number of Effective Pixels that are processed and stored as additional detail in the Recorded Pixel file.
Super CCD SR (Sensitivity and Range): Uses a combination of small and large octagonal-shaped pixels to further enhance color accuracy, while improving detail in the areas of shadows and highlights, much like traditional film
1/2.7 "
|
| Light exposure correction |
-2EV to +2EV in 1/3EV Steps |
|
Camera shutter speed
|
|
Determines the length of time the shutter lets light pass through the lens to the CCD. Shutter speed and aperture together determine exposure.
2- 1/1000 s
|
| Flash |
Auto, Anti-red-eye, On, Off |
| Built-in flash |
 |
| Compatible memory cards |
16 MB Memory Stick |
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
1.5"
|
|
Camera viewfinder
|
|
Window in the camera through which a photographer views the picture. Used for choosing, composing, and often focusing the image.
Optical Viewfinder (Real Image): The photographer looks through a transparent window to frame and focus the image. The photographer is seeing the real image, through the window of the viewfinder.
Digital Viewfinder: An LCD display built into a camera that gives a digital view of where the camera is pointing. It's used to compose and focus the image.
Optical
|
|
|
Self-timer
|
|
description of the selftimer of the camera; like time of shutter delay; remote control etc
10 s
|
| Metering |
Multi-Segment, Spot |
| Power requirements |
InfoLithium (NP-FC10) & charger |
| Resolution |
1600x1200 pixels |
|
Dimensions W x D x H
|
|
Dimensions of the produkt (Width x Depth x Height) in millimeter.
114 x 52 x 38
|
|
Weight
|
|
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
214 g
|
|