|
Taking shots of the kids on a family vacation. On an airplane drowning out jet turbine noises with soothing MP3s. Making some hilarious movies of friends with a digital camcorder. Everywhere you look, digital media becoming an essential part of our everyday lives. Wouldn't it be great to not only conveniently take large amounts of digital storage with us, but also backup our precious photos, videos,
...
More>>>
and music on the road, without the need to haul around a bulky laptop? Now you can. Thecus Technology is proud to introduce the YES nano N1050 OTG Photo Bank. Featuring on-the-go backup, large storage capacity, and USB 2.0 connectivity, the YES nano N1050 delivers digital storage that’s as active as you are.
The first thing you'll notice is just how small the YES nano N1050 is. Measuring a scant 124 x 75 x 13mm, the YES nano N1050 is barely larger than the 2.5" hard disk it houses. With 2.5" hard disks reaching 100GB or more, the YES nano N1050 can accommodate massive storage in form factor that fits quite handily in a purse or coat pocket. With the included protective carrying case, the YES nano N1050 makes a perfect travel companion. What's more, because the YES nano N1050 accepts standard 2.5" IDE hard disks, users can select the capacity that's right for them. A casual user that needs to bring files home from the office? A 20GB hard drive will suffice. A multimedia mogul that can't seem to let go of their digital camcorder? Slap in a 100GB hard drive and capture that Oscar-worthy documentary. With the YES nano N1050, the choice of capacity is yours.
Despite its diminutive measurements, this pint-sized wonder is a dual function device that allows you to not only stores large amounts of digital media, but also enables you to backup your digital devices on-the-go. Imagine never worrying about running out of storage or losing your data while on the road! Digital camera or camcorder almost out of space? Simply plug your digital device into the YES nano N1050's USB 2.0 port, press the copy button, and backup your entire memory card or internal hard disk at speeds of 480Mbps - no computer necessary! With virtually unlimited storage space, the YES nano N1050 grants not only peace of mind, but also the freedom to unleash your creativity.
The YES nano N1050 is built for ease-of-use. Transferring files and from the YES nano N1050 is a simple affair, involving the plugging of a USB cable and the flick of a switch. Backing up files on-the-go requires plugging in a USB device and pressing a button. Engineered for simplicity, the YES nano N1050 lets you spend less time fussing, and more time enjoying. But what about running out of juice on the road? The YES nano N1050 has you covered. The YES nano N1050 can be powered by a USB-DC power cord, or via the included external power pack. Best of all, the external power pack accepts standard AA batteries, ensuring that the YES nano N1050 is ready whenever you are.
<<<Less
|